{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Configuration Manager Tool v9 fails while reading Power Monitoring Expert v9.0 system
Issue
Configuration Manager Tool v9 fails with below errors while Read from System’ in PME v9 machine.

||Warning||None||||Could not find manifest file: D:\1.PME 9.0 Configuration Management Tool\bin\MasterFileLists\PowerMonitoringExpert\9.0\DataCenter\en\config.csv||None
||Warning||None||||Could not find manifest file: D:\1.PME 9.0 Configuration Management Tool\bin\MasterFileLists\PowerMonitoringExpert\9.0\Healthcare\en\config.csv||None



Environment
Power Monitoring Expert v9.0 system read by Configuration Manager Tool v9.


Cause
When older PME versions are upgraded in-place this registry will remain and when cause this issue when old systems are DataCenter or Healthcare. From PME 9 onwards we don’t have any such PME versions anymore.

Resolution
Open RegEdit and go to the path > “HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\Schneider Electric\Power Monitoring Expert\9.0” and delete key "SolutionBuild" which contains value either 'DataCenter' or ' Healthcare'.

Schneider Electric Saudi Arabia