Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EcoStruxure Hybrid DCS [2018] How to fix the error that 'A time stamped variable must be mapped on the address %SW73.7'
  1. Issue
Customer encountered an error “A time stamped variable must be mapped on the address %SW73.7 (SOE uncertain)” when building the executable.
  1. Product Line
Hybird DCS 2018
  1. Environment
Hybird DCS 2018, Unity Pro V13.0, Win10 64Bit SP1
  1. Resolution
  1. Refine the built program, create a test variable Bool type and assign address %SW73.7.
  2. Right click and go to customize columns, select time stamping and enable for this variable, and make it both edges.

After all, building the executable to check whether the error has been fixed.