Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does BMXDAI1604 module hold the last value when powered off?
  1. Issue
Customer observed that in BMXDAI1604 module the last value is held in Unity software even when the 110V power supply is off, whereas there is no LED indication on Modules and is only normalized when power is back. (Refer to snapshots below).
  1. Product Line
Control Expert V14.0, BMXDAI1604


  1. Environment
Unity Pro version - V13.1 without hotfix
CPU version BMEP586040: SV-2.7
CRA Version BMECRA31210: SV-2.3
  1. Resolution
This issue is caused by BMECRA31210 SV2.3.
There is no such issue with BMECRA31210 SV2.31 and SV2.4. Upgrading the firmware of CRA will fix this issue.
  1. FAQ Applicable Conditions
Additionally, in the Firmware History of CRA SV2.31, it indicates this similar issue has been fixed for BMXDAI1615.