Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to send control command to PowerTag C A9XMC1D3 and A9XMC2D3 devices through PowerTag Link web page ?
Command with web page is not possible due to Cybersecurity reasons (HTTP requests).

You send a command with the following methods :
  • EcoStruxure Power Commissioning
  • Modbus write requests on Register Adress 0x90BA (Register Number 37051)