Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to obtain scan execution times in M340 and Quantum PLC

Article available in these languages: Japanese

Issue
What are scan execution times in M340 and Quantum PLC

NOTE (definitions):
- The amount of time it takes to perform one cycle is referred to as scan time
- Cycle means perform all configured, programmed and enabled activities in a fixed sequence as fast as possible

Product Line
Unity Pro (software)
M340, Quantum (PLC)

Environment
System Addressing

Cause
Trouble shooting purpose

Resolution
Scan execution times can be obtained using system objects:

  • %SW30    last scan
  • %SW31    longest scan
  • %SW32    shortest scan

You can use an animation table to look at the values:

Screenshot of animation table

You can also see those values in the PLC screen when online with the PLC

PLC Screen demo

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre