Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
TMAHOL02 battery door for the M221 controller.
Issue:
The M221 battery doors are not sold in the US.

Product line:
M221

Cause:
The customers threw out the package with the battery and battery holder.

Resolution:
As of 1/20/21 the battery door is now sold in lots of 2 under part number TMAHOl02