Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I set the deceleration time on a ATV320?

Issue:
Setting deceleration time on a ATV320.

Product Line:
ATV320

Resolution:
Parameters described in this page can be accessed by: DRI- > CONF > FULL > SIM
Goto Configuration Mode (ConF)  > Enter
Goto to FULL > Enter
Goto SIM > > Enter
Goto deC [Deceleration]  default  3.0s
Set desired value for deceleration time.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.