Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you power the Altivar 212 drive using the DC bus?
Issue:
Is there a way to use the ATV212 drives with a Bonitron DC power supply for a site that only has single phase available?

Product line:
Altivar Building ATV212 Altivar 212

Cause:
Application single phase supply

Resolution:
The ATV212 are not suitable to be powered with single phase or by the DC bus.  The DC power terminals are present on the drives; however, they're covered with glue to prevent connection.  The DC bus terminals can only be used for measuring the DC bus.