Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I see the drive output frequency on ATV630?
Issue:
Where can I look in the ATV630 HMI to verify the drive running speed?

Product Line:
ATV630. ATV650, ATV660

Environment::
All serial numbers

Cause:
Verify the speed and reference

Resolution:
Goto Main menu > Complete Setting > Drive parameters >
Ref Freq  (target speed)
Motor Freq (drive output speed)