Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What would cause the ATV320 drives to trip on OSF faults on powerup?

Article available in these languages: Spanish

Issue:
The ATV320 drives to trip on OSF faults on powerup?

Product Line:
ATV320

Environment:
All serial numbers

Cause:
Can not clear fault

Resolution:
To clear the OSF fault on powerup:
Set  UrES [Mains voltage]  to correct value of the line supply voltage.
Parameters described can be accessed by:

DRI- > CONF > FULL > FLT- > CLL
USb- [UNDERVOLTAGE MGT]   > enter
UrES [Mains voltage]  > enter
Enter the correct line voltage
If set to 380V change to 460V (or appropriate voltage per your application)