Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I set my ATV320 internal fan to run all the time?
Issue:
Can I set the drive fan to run all the time?

Product Line:
ATV320

Environment:
All model numbers, all serial numbers

Cause:
N/A

Resolution:
You can change the Fan Mode from standard to always.  Press enter on RDY, then turn knob clockwise to Conf and press enter.  Scroll down to FULL and press enter, then turn knob clockwise to SET and press enter.  Scroll down to FFN and press enter, and change std to run.