Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to having FTP data publishing more frequent that 1 hour on the COM’X 510?
Issue
Is it possible to having FTP data publishing more frequent that 1 hour on the COM’X 510?

Product Line
COM’X510

Environment
FTP Data Pushing

Cause
The maximum default option for FTP data publishing interval is 1hour, but a shorter interval is needed.

Resolution
There is no a way to publish more frequently than once an hour. The available Publication frequency are: Every hour, Every 2 hours, Every 3 hours Every 4 hours, Every 12 hours, Every day, Every week, and Every month.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre