Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ATV340 -When setting up the drive, using Somove, how do I assign a Preset speed to a digital input?
Issue:
How do I assign a Preset speed to a digital input, in Somove?

Product Line:
Software

Environment:
Somove

Cause:
In the I/O menu digital input assignments are grayed out. Unable to change.

Resolution:
To setup Preset speeds:
Go to the Preset speed function and assign the desired digital input.