Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME 2020 - Diagnostic Viewer > Service Diagnostics > Communication Server > Tree States shows "BAD"

Issue:
When you navigate to Diagnostic Viewer > Service Diagnostics > Communication Server you see the tree state shows "BAD" as shown in the below screenshot.
a

Product Line:
Power Monitoring Expert 2020

Environment:
Diagnostic Viewer

Cause:
This is a bug with the PME Diagnostic Viewer. It is just a display issue and does not affect PME in any other way.

Resolution:
It will be addressed in PME 2020 CU1

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre