Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EPO 2024 Demo and Highlights
Issue
There is a new version of EPO and a user would like to know the details.

Product Line
EcoStruxureTM Power SCADA Operation (EPO)

Environment
EcoStruxureTM Power SCADA Operation (EPO) 2024

Resolution
The EPO 2024 Demo can be launched from the following link
https://www.se.com/ww/en/work/solutions/power-management/demos/
User name / password: demo / demo
User name / password (to demonstrate dark mode): demodark / demo
(see screenshot below with mark-ups for launching EPO demo)

Some highlights of the new EPO online demo as compared to previous demo:
  • As you would expect, use of new native HTML5 functionality including pan/zoom graphics, alarms, waveforms, etc.
  • Ability to interact with demo independently of other users
  • Ability to toggle between IEC and ANSI graphics via green gear icon on Diagram pages
  • On Data-center 1-line Diagram, new scenarios & simulations
  • More waveforms
  • Saved reports
  • Microgrid Operation graphics / templates
  • Multi-source 1-line colorization (eg: Utility + PV = unique color) in the Microgrid diagrams

mark-ups for launching EPO demo