How to Logout at the Easergy Micom P63x relay properly ?
Issue/description:
Logout at the Easergy Micom P63x realy properly
Product family:
Easergy Micom P63x
Resolution:
For security consideration, it would be better to logout the IED once the configuration is done.
The user can be logged out with 'HMI Logout' in the menu tree: 'Par/Conf/CS' or using the softkey 'LOGOUT'.
Additional info.to Logout at Easergy Studio:
Right-click on the device name and select Log Off.
● In the Log Off confirmation dialog click Yes.