Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Could you support with Relay pack for SE7300/SE8300 mixed voltage fan coil applications?
In combination with the SE7300/SE8300 Series Room Controllers, the SC1300 and SC2300 allow control of a fan-coil requiring mixed voltage for the following:
• line voltage for the 3-speed fan control (SC1300 is 120V unit and SC2300 is 220/240V unit)
• low voltage for the valve control

Refer to Fan Control Center Installation Guide for detailed wiring instructions:
Fan Control Center - Installation Sheet