How can we help you today?

How can we disable a physical port in Easergy MiCOM P63x relays?

Issue/description:

Sisable a physical port in Easergy MiCOM P63x relays

Product family:

Easergy MiCOM P63x relays

Resolution:

It is possible to disable unused physical ports for security reason.
The physical ports can be disabled by using Easergy Studio or the front panel.
This can’t be done by the CAE. An Engineer-role is needed to perform this action.
COMM1 section:
● Allows to disable commands.
It can be disabled with 'Command blocking' in the menu tree: 'Par/Func/Glob/
COMM1'.

COMM2 section:
● Allows to disable commands and measurements. If both are disabled, the complete interface is disabled.
It can be disabled with 'Command blocking' or 'Sig./meas.val.block' in the menu tree: 'Par/Func/Glob/COMM2'.

IEC section:
● Allows to disable the physical interface A/B or A (if available).
● Allows to disable the physical interface C.
The physical ports can be disabled with 'Block Port A/B' or 'Block Port C' in the menu tree: 'Par/Conf/IEC'.

PC section (IEC 103):

● Allows to disable commands and measurements. If both are disabled, the complete interface is disabled.
It can be disabled with 'Command blocking' or 'Sig./meas.val.block' in the menu tree: 'Par/Func/Glob/PC'.

Schneider Electric Saudi Arabia
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
  • Product Documentation