Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
what is the Maximum number of Modbus devices can be added to EcoStruxure Building Expert MPM?
You can add the following number of Modbus Devices:
  • 33 (or a combination) of the following acti9 Devices:
    • ACT24 iCT Contractor
    • iOF + SD24 Circuit Breaker
    • Reflex iC60 Circuit Breaker
  • 30 Power Meters
You can add a combination of acti9 Devices and Power Meters as long as the total number of Devices does not exceed 49.
Starting with version 2.18, users can now add generic Modbus RTU devices in Building Expert. The new feature is available in the Add Device menu. The device allows a user to upload a .csv file containing register information of a Modbus RTU communicating device, however only holding registers are supported at this time. Building Expert then creates the required Objects from the files and communicates them to the device. A Maximum of 5 Generic Modbus RTU Devices can be added.