Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PLC different memory usages in EcoStruxure Control Expert explained

The memory usage function is used to view :

  • The physical distribution of the controller memory (see EcoStruxure™ Control
    Expert, Program Languages and Structure, Reference Manual) (internal memory and
    memory card)
  • The space consumed in the memory by a project (data, program, configuration,
    system
  • It can also be used to reorganize the memory where possible

Note : The memory usage screen is not available in simulation mode. This screen is only available in standard mode for a built application.
The screen is accessible if the application is built and is in the NOT BUILT state due to a program modification, but it corresponds to the previously built application. Modifications are taken into account at the next build

To access the memory usage details of the controller :

  1. Activate the PLC > Memory Consumption... command to display the corresponding screen. The
    memory usage statistics of a project can only be accessed if you have generated its executable in
    advance
  2. If you want to reorganize the memory to optimize it, activate the Pack command

M580

Safety

M340

Legacy

Description of the parameters :

Parameters

Memory re-organization :

Memory re-organization is activated using the Pack command. Memory re-organization can be performed in online or offline mode (even if the controller is in Run or in Stop).

Note : Certain blocks cannot be moved in online mode. You can attain a lower level of fragmentation by re-organizing the memory in offline mode