Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where to find EDS file for PM5560 meter?
Issue
EDS file is required to configure PM5560 meter to communicate over Ethernet/IP CIP protocol. From where it is possible to get this file?

Product Environment
PM5560 with Ethernet/IP CIP protocol

Resolution
EDS file is available along with the f/w release package. It is possible to download the latest f/w installation package from the below-mentioned website.

https://www.se.com/ww/en/download/