Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to replace internal battery of PM800 meters?
Issue
The meter is losing RTC information (date and time) without the Aux power supply.

Environment
PM800 series meters

Cause
This may happen with an old and drained internal battery.

Resolution
PM800 series meters are no more in offer. The sale for this product is ended. It is obsolete and not serviceable. The factory no longer offers a battery replacement service and there is no way to replace the battery in the field.