Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Understanding Virtualization Features in FlexNet Publisher

Issue
Challenges in software licensing

Product Line

Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020

FlexNet Publisher 2018 R1 (11.15.1) and later

Environment
Licensing

Cause
This White Paper describes virtualization challenges in software licensing and the facilities available in FlexNet Publisher for operating licensing models in a virtualized environment.

Resolution
Virtualization in FlexNet Publisher

Schneider Electric Saudi Arabia

Attachment(s)
FNP_Virtualization.pdf [324.02 KB]