How can we help you today?

In IONSetup, Is there any way to view device timestamps in a different time zone than my PC?

A new feature, ION Setup will now attempt to detect a device’s programmed time zone and prompt the user if it is different than the PC.
TimeZone Setup


The automatic time zone detection can be enabled/disabled from the Tools -> Options menu on the View tab.
TimeZone Options


Once set, the selected time zone setting can be modified using the Device Properties -> Time Zone tab.

Device Properties
All UTC time stamps will then use the selected setting when showing device data (meter local time will display as it is).

Schneider Electric Saudi Arabia