Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert - SQL script to truncate a table in ION_Data Database
Issue
A SQL script is needed to delete "ALL" historical data from the ION_Data database faster.

Product Line
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020


Environment
SQL Server Management Studio

Cause
The "Truncate" query is a faster way to remove all data from specific tables that holds historical data. Truncate is faster and uses fewer system resources than a regular trim job.
Note: Truncate removes "ALL" entries from a table once it is executed.

Resolution
*Warning: Irreparable database damage can occur. Databases should be backed up prior to performing this procedure.*
*Warning: This procedure is recommended to be deployed by users familiar with Databases.*


The following are the scripts to remove "ALL" entries from DataLog2, EventLog2, and WaveformLog2 respectively.

1-
USE ION_Data
TRUNCATE TABLE DataLog2


2-
USE ION_Data
TRUNCATE TABLE EventLog2


3-
USE ION_Data
TRUNCATE TABLE WaveformLog2

Schneider Electric Saudi Arabia

Attachment(s)
WaveformLog2.txt [41 Bytes]
DataLog2.txt [37 Bytes]
EventLog2.txt [38 Bytes]