Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to manage the import/export of the Symbol list in EcoStruxure Machine Expert - Basic?
Depending on Microsoft Excel and Windows settings, the .csv file created when exporting the Symbol list from ESME-Basic* could not be displayed as expected in MS Excel.
Likewise, we could get some errors when importing the Symbol list in ESME-Basic.

Example of error during the import:


Hereafter, a summary of the different combinations:

1) List Separator in Windows settings => Comma: “,”

Export options in ESME-Basic:
Unicode + Semicolon => need to adapt in Excel by selecting semicolon as delimiter => save as .csv-utf8 file => import in ESME-Basic by selecting semicolon => Error
Unicode + Comma => need to adapt in Excel by selecting comma as delimiter => save as .csv-utf8 file => import in ESME-Basic by selecting comma => OK
ANSI + Semicolon => need to adapt in Excel by selecting semicolon as delimiter=> save as .csv file => import in ESME-Basic by selecting semicolon => Error
ANSI + Comma => correctly displayed in Excel without doing any adaptation => save as .csv file => import in ESME-Basic by selecting comma => OK


2) List Separator in Windows settings => Semicolon: “;”

Export options in ESME-Basic:
Unicode + Semicolon => need to adapt in Excel by selecting semicolon as delimiter=> save as .csv-utf8 file => import in ESME-Basic by selecting semicolon => OK
Unicode + Comma => need to adapt in Excel by selecting comma as delimiter => save as .csv-utf8 file => import in ESME-Basic by selecting comma => Error
ANSI + Semicolon => correctly displayed in Excel without doing any adaptation => save as .csv file => import in ESME-Basic by selecting semicolon => OK
ANSI + Comma => need to adapt in Excel by selecting comma as delimiter=> save as .csv file => import in ESME-Basic by selecting comma => Error


Through these different tests, we can see the error appears when the list separator of Windows is different from the separator selected in ESME-Basic.
When handling Unicode file, take care to select csv-utf8 format when saving as the .csv file in MS Excel.



Note 1: How to change the List separator in Windows?




Note 2: How to change the Delimiter in MS Excel?




*ESME-Basic: EcoStruxure Machine Expert - Basic