Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Function Implicit Type Conversion

Issue
User can be found an issue working with type to type operation at Control Expert.
implicit conversion

Environment
Control Expert
Resolution
As per default the function Enable Implicit Type Conversion is not checked when the user create a new project. Then this function must be checked to avoid errors with the application. To activate this function:
1- Go to Tools > Project Settings > Program > Languages > Common
2- Enable implicit type conversion
For further details, see the document attached.

Schneider Electric Saudi Arabia

Attachment(s)
Implicit Type Conversion.pdf [252.23 KB]