Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the Modbus ASCII serial transmission mode supported in SmartX Servers?
Issue:
Modbus ASCII serial transmission mode support in EcoStruxure Building Operation SmartX servers.

Product line:
EcoStruxure Building Operation, Automation Servers (AS, AS-P, AS-B)

Resolution:
SmartX servers (AS, AS-P, or AS-B) support both RTU and ASCII serial transmission modes.  In WorkStation, you can select either one of these modes in the Framing mode section of the network properties.
To ensure that all devices on a Modbus serial line can communicate with each other, you must set the transmission mode (and serial port parameters, for example baud rate and parity) to be the same for all devices.

Machine generated alternative text:Modbus Master Network Basic General Information Status Information Configuration Settings Advanced Semantics References Framing mode Baud rate Parity Stop bits J-Bus mode Port reference ASCII Even Auto Null Close

For more information refer to below WebHelp article:
https://ecostruxure-building-help.se.com/bms/Topics/show.castle?id=6943