Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the compatible SmartX IP controller device firmware version for my EBO installation?
Issue:
Compatibility between SmartX IP controller devices firmware and EBO software version.

Product Line:
EcoStruxure Building Operation, SmartX IP Controller devices

Resolution:
The SmartX IP controller devices shipped from the factory may not have the latest firmware installed. It is essential to verify that the controller has the latest firmware build loaded for the EcoStruxure Building Operation "EBO" version build being used before programming the controller. The below table contain the supported SmartX IP controller devices firmware for each EBO release.
Machine generated alternative text:SmartX IP MP/RP and IP-IO Series Controller Versions EBO Versions "2.0.1/2/3 v2.O.4 v3.o.x V3.1.x v1.OO.Ox Supported + Tested Supported + Tested Not supported Not supported v2.oo.ox Not supported Supported + Tested Supported + Tested Supported + Tested v3.01 .ox Not supported Not supported Not supported Supported + Tested
* New v3.2 features are not supported when used with EBO v3.1.x.
Note: RP-C is only supported on EBO 3.0 and later