Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to mount/remove Modbus RTU Slave base Module for MULTICAL 62/601/602/801?
Issue:
Installation instruction for Modbus RTU Slave base Module (MAMODBASE).

Product Line:
Heat Meters

Resolution:
The Modbus base module (PN: MAMODBASE) for MULTICAL® allows simple integration from heat, cooling, and water meters to a building management system, using standard Modbus serial communications.
The module is mounted within the MULTICAL itself and is used for data transfer from MULTICAL heat, cooling, and water meters to external Modbus systems.

The module is mounted in the connecting base of the meter in the following way:

The module is removed in the following way:
The module is released by pressing the ”Release” upwards and at the same time drawing the connection terminals at the top of the module.

Electrical connection:
The Modbus module is automatically connected with the meter via the 6-pole connector just below the ”Release” when the top part of the meter is mounted.
The RS-485 cable is connected via the cable inlets on the connecting base.

For more information, please refer to the module specification sheet:
https://ecobuilding.schneider-electric.com/search?documentUUID=33f562ac-6239-45fc-b1a5-a17dc61eb54e&title=Modbus RTU Slave Module for MULTICAL 62, 601, 602, 801 Specification Sheet