Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Scada Operation (PSO) 2020 - Migrating an existing diagram built on the legacy Graphics Builder to the new Graphics Editor
Issue
A user would like to migrate an existing diagram which was build on the legacy Graphics Builder to the new Graphics Editor and continue working on it.

Product Line
EcoStruxure™ Power SCADA Operation 2020

Environment
Graphics Editor

Cause
The diagrams from the legacy Graphics Builder will not function on the new Graphics Editor.

Resolution
There is no migration tool for graphics currently. The graphics will have to be re-done from scratch.
However, the legacy graphics can still be created and maintained by installing the Citect graphics builder.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre