Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the function of External neutral voltage tap (ENVT) in Compact NSX?
Issue: ENVT in Compact NSX.
Environment: Compact NSX.
Resolution: This connection is required for accurate power measurements on 3-pole circuit breakers equipped with Micrologic 5 / 6 E trip units in installations with a distributed neutral. It can be used to measure phase-neutral voltages and calculate power using the 3-wattmeter method.
The phase to neutral voltage is always available for 4 poles circuit breakers, while for 3 poles circuit breakers, the connection of the Micrologic 5 / 6 E to the neutral using ENVT is a must. This is to guarantee the accuracy for the active power measurement.
Compact NSX 3-pole circuit breakers come with a wire installed on the device for the connection to the ENVT.