Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Configure the BMXNOR0200 for DNP3 communications with redundant server
Issue
Configure the BMXNOR0200 for DNP3 communications with redundant server

Product Line
BMXNOR0200

Environment
Windows 7, Windows 10

Resolution
The purpose of this video is to demonstrate how to configure the BMXNOR0200 to communicate with multiple DNP 3 servers