Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does SE8350 room controller fan stay in low speed instead of shutting down when there is no demand?
Issue:
Fan connected to SE8350 room controller stays running at low speed when there is no demand

Product Line:
SE83500 room controllers

Resolution:
There are three possible causes:
  1. The “Fan mode” is set to “Low” instead of “Auto”.
  • Auto selection will activate fan on demand.
  1. The “Auto Fan func.” is set to “AS”.
  • Change the setting to “AS / AD”.
  • AS: In Occupied, Standby, and Override modes, the Fan stays ON at low speed even if there is no demand for Heating or Cooling. In Unoccupied mode, the Fan turns Off when there is no demand for Heating or Cooling.
  • AS/AD: In any Occupancy mode, the Fan turns Off all speeds when there is no demand for Heating or Cooling.
  1. The Dehumidification is activated.
  • If dehumidification is not required, set the “Deh. lockout” parameter to “Disable”.