Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to resolve the issue that occurs when the user tries to transfer a Control Expert application into an M580 PLC that contains a lower exec firmware version.
Issue
This video demonstrates the issue that occurs when the user tries to transfer a Control Expert application into an M580 PLC that contains
a lower exec firmware version.

Product Line
Control Expert

Environment
Windows 10

Resolution
This video demonstrates the issue that occurs when the user tries to transfer a Control Expert application into an M580 PLC that contains
a lower exec firmware version.