Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Power Monitoring Expert 2020 or Energy Expert v3.0 Integration Utility fails to generate the EBO ‘Workstation Import file'.

Issue
Power Monitoring Expert 2020 or Energy Expert v3.0 Integration Utility fails to generate the EBO ‘Workstation Import file' when selected authentication method as ‘Automatic PME or Windows Authentication’.

Environment
Power Monitoring Expert 2020 or Energy Expert v3.0 Integration Utility

Cause
A bug (# 104855) in the tool has been logged for this issue.

Resolution
Below workaround can be applied to fix the issue.
1> Using ‘Energy Expert v3.0 Integration Tool’ generate the workstation import file by selecting ‘Manual PME Authentication’.
aa

2> Import the workstation import file (generated from first step) in EBO and this will create required configuration related to PME.

3> Now generate PME Web links (for Dashboard/using web tool (Generate Authentication URL) by using URL 'https://<YourServerName>/Web/MUT'(refer below screen-cap for the same).
For more information on ‘Creating Diagrams, Reports, and Dashboards links in Building Operation’ refer document ‘Power Monitoring Expert 2020 System Guide’ page#1676 (https://www.se.com/ww/en/download/document/7EN02-0426/ )
aa

Generate Destination URL:
/Web for the PMEWeb Applications Settings page.
/Dashboard for the PME Dashboards page.
/Reporter for the PME Web Reports page.


4> Copy authentication URL from previous step and replace same in EBO configuration against each tab configurations.

Note: This bug will be fixed in next version of PME/EE.