Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to connect PT100 RTD to ATS48?

Unfortunately, the PT100 RTDs are not compatible with the Altistart 48.

Only the PTC thermistor could be connected to PTC1 and PTC2.