Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
XU1K3LLXXRCC and XU2K0LLXXRCC Firmware Upgrade via NMC times out


Issue:

XU1K3LLXXRCC and XU2K0LLXXRCC Firmware Upgrade via Network Management Card times out and is unable to complete

Product Line:

Smart-UPS Industrial

Environment:

XU1K3LLXXRCC and XU2K0LLXXRCC, All Serial Numbers

Cause:

When upgrading the firmware via the Network Management Card, there is a delay in transferring the data to the UPS.
This causes the update to time out and fail.

  • The time-out error occurs while Receiving Firmware image is in progress.
  • The percentage at which the time out error occurs varies from unit to unit.



The LCD Display on the UPS will look like this:
img



The NMC Web interface will display this error:

img

Resolution:

If you experience this issue, you can upgrade the UPS using a USB Thumb Drive rather than via the Network Management Card.
Instructions and the latest firmware image can be found in APC FAQ ID FA402857

Note: Subsequent UPS firmware updates can be performed via the NMC; however, the time to perform the update may increase by 10 minutes.