Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do you have 27R function (Remanent voltage / Anti-Backspin) function in Micom motor protection relay P24x relay range ?

Description:
27R function (Remanent voltage / Anti-Backspin) protection function in Micom P24x relay

Product family:
Micom 24x relays

Resolution:
27R function (Remanent voltage / Anti-Backspin) need to have option for VT connection = 2VT + Remanent.Yes, this option is available in Micom P24x