Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is cable type for connection between motor and softstarter PTC terminal block ?
Some practical recommendations for the type of cables that should be used are as follows:

- Distances ≤ 20 m – Standard parallel cable is acceptable
- Distances ≥ 20 m, ≤100 m – Twisted pair cable is necessary
- Distances ≥ 100 m – Screened twisted pair (STP) cable is necessary
- High level of interference  – Screened twisted pair (STP) cable is necessary