Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why it fails to import variables into EOTE after editing the CSV file in Excel
  1. Issue
Why it fails to import variables into EOTE after editing the CSV file in Excel.
  1. Environment
EcoStruxure Operator Terminal Expert 3.1 or later.
  1. Resolution
After editing the .CSV file in Excel, the format is modified, then it will not work when importing variables.
User can edit the original .CSV file in NotePad++, then import the .CSV file into EOTE.
Or edit the original .CSV file in Excel but save it as a TXT file, then import the TXT file into EOTE.


  1. FAQ Applicable Conditions
FAQ applies to EcoStruxure Operator Terminal Expert 3.1 or later.