Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to show UNIX time on a mimic in Geo SCADA

DISCLAIMER

The example below is intended to demonstrate one or more features or methods and is presented as a configuration example only. Schneider Electric assumes no liability for the use or application of this example or any portion thereof.



The Unix time is the number of seconds that have elapsed since January 1, 1970 (midnight UTC/GMT), not counting leap seconds. Some customers asked how to show the date from that number on Geo SCADA.
Given the "Unix time", the following expression will show the appropriate time stamp ("NSecs" is a variable that contains the "Unix time" number in the example below, note also that the "Date/Time" text box was formatted to show dd/MM/yyyy HH:mm:ss):

#1 January 1970# + ".NSecs"/86400

Animations

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: