Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to update the exec firmware on a BMENOR2200.
Issue
How to update the exec firmware on a BMENOR2200.

Product Line
BMENOR2200

Environment
Ecostruxture Automation Device Maintenance

Resolution

Use the following steps to update the exec firmware.

  • Place the module into non secure mode.

iy

  • Open and log into BMENOR2200 web server homepage to ensure that it is reachable.
gf




  • Start the 'EcoStruxure Automation Device Maintenance' software.
gfg




  • Click on the Add button.
dgg



  • Enter the NOR022 IP address.
  • Select 'Identification via' as  'Any Method'.
  • Click on OK.
evge



  • Click on 'Yes' in the 'Unidentified Device' pop-up window.

egg


  • Verify that the NOR2200 is reachable (The dot next to 'Unidentified Device' should change will be shown as yellow.
egvge




  • Select the Data Package version for the NOR2200.
geg




  • Click on the red 'Trust' icon.
. gege



  • Select the 'Trust the server certificate temporarily for the current session' checkbox. (Note:   If this step is skipped, you will not be able to connect to the NOR2200.)
  • Click on the 'Trust Device Certificate' button.

get


  • Click on the 'Device Login' icon.

etgt


  • Enter the username and password.
  • Click on 'Save'.

etgegt



3tgb


  • The yellow dot will turn green.
  • Click on the Green dot.

gtev


  • Click on the 'Update Firmware' button.
rweg



  • The exec firmware will start to load.

ergtrv