How can we help you today?

Power Monitoring Expert v8.2/v9.0 /PME2020: CM2000 driver provides incorrect firmware version

Issue
PME 2020 and in previous versions show the firmware version of the CM2000 series meters incorrectly, both in Vista and in the Diagnostics. This intern has an impact on Power Advisor as well.

Environment
Power Monitoring Expert v8.2/v9.0 /PME2020

Cause
Bug with the PME driver.

Resolution

Note: Refer Readme.txt document available with each version to know about the steps to apply the fix.

For more information on
How to determine the firmware version of CM2000 series meters via Front Panel or remotely by software’ refer FAQ - FA211882
What is the minimum firmware requirements for Powerlogic meters in StruxureWare Power Monitoring Expert?’ Refer to FAQ - FA210274

Schneider Electric Saudi Arabia