Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the configuration file from a Com'X 200/210 be restored into Com'X 510?
Issue
Can the configuration file from a Com'X 200 or Com'X 210 be restored into Com'X 510?
Environment
Com'X 200, Com'X 210, Com'X 510
Cause
On the site, the customer likes to replace the existing Com'X 200 and Com'X 210 with Com'X 510 but retain the configuration of those retiring 200s and 210s.
Resolution
A configuration file from a Com'X 200 or Com'X 210 cannot be applied to a Com'X 510 and a configuration file from a Com'X 510 cannot be applied to a Com'X 200 or 210.