Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which panels are needed for Smartlink ELEC?

Electrical panels with 24 modules per row (18mm width per module).
Smartlink EL B product is installed between 2 rails with minimum space of 150mm.
Please refer to e-catalogue on web link: www.se.com/br>