{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the Altivar ATV28 drives repairable?
Issue:
Wondering if the Altivar ATV28 drives, are repairable?

Product Line:
ATV28

Environment:
All

Cause:
Repair

Resolution:
No, the Altivar 28 drives are not repairable. Since ATV28's are already obsolete, the recommendation is to replace the drive with a present drive.


Schneider Electric Saudi Arabia