Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: Why would the ATS48 display an nLP Status?

Issue:
nLP Status on ATS48

Product Line:
Altistart ATS48

Cause:
No Mains voltage present on the input of the soft starter before start.

Resolution:
NLP means No Line Power. This indicates there is no mains power applied to the starter`s L1 - L2 - L3 terminals.
This may be due to a trip condition, but for a device with a line contactor, this is the normal OFF state.

,