Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the gain adjustment do for the ATV28 drive?
Issue:
Gain adjustment function on the ATV28.

Product Line:
ATV28

Environment:
All

Cause:
N/A

Resolution:
The gain function allows adjustment of the response time of the drive controller to sudden changes in the motor load. Decreasing the gain parameter slows the response time of the drive controller. Increasing the gain parameter makes the drive controller respond more quickly to load change. This parameter should be increased in applications where the undesirable changes in motor speed occur due to changes in motor load. Applications that have fast cycle times or high torque requirements may require an increase in gain.


Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre