Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for main control board for ATV66 drive?
Issue:
Main control board part number for ATV66 drive

Product Line:
Altivar 66, ATV66

Environment:
All

Cause:
Parts

Resolution:
There are 3 possible kit part numbers:

For ATV66U41N4 to ATV66D79N4 and ATV66U41M2 to ATV66D46M2 except ATV66D23M2S264 use VX4A66CK1;

For ATV66D23M2S264 use VX4A66CK1S260;

For ATV66C10N4 to ATV66C31N4 use VX4A66CK2

In all  of the kits listed above, the keypad is included.

Please note:
The VX4A66CK1 and VX4A66CK2 are both now obsolete.

Schneider Electric Saudi Arabia

Attachment(s)
ATV66 Main Control Board Parts FAQ Template.xlsx [13.26 KB]
Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: